FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Electronic bypass function
FAQ
Electronic bypass function
There are two patterns of the automatic bypass sequence in the electronic bypass operation sequence. What is the proper use?
- Category :
Answer
With the automatic bypass sequence (Pr.139 ≠ 9999, Pr.159 = 9999), the motor operation is switched to commercial power supply operation when the output frequency reaches Pr.139 and the inverter is used only for the acceleration/deceleration operation. With the automatic bypass sequence (Pr.139 ≠ 9999, Pr.159 = 9999), the motor operation is switched to commercial power supply operation when the output frequency reaches Pr.139. When the frequency command becomes less than the difference between Pr.139 and Pr.159, it is automatically switched to inverter-driven operation at the frequency by the frequency command. Therefore, use the commercial power supply for high-speed operation, and inverter for low-speed operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700