FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > AM terminal output
FAQ
AM terminal output
Using two inverters, I want to use the voltage signal from the terminal AM of the first inverter as speed command of the second inverter. And also I want to set the output of terminal AM to 10 VDC when the first inverter operates at 70 Hz. How should I configure the setting?
- Category :
Answer
Set Pr.55 (Frequency monitoring reference) of the first inverter to 70 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700