Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21255
  • Release Date : 2018/08/22 16:26
  • Print

Automatic restart after instantaneous power failure

I want to use automatic restart after instantaneous power failure function in the A700 series, but the inverter cannot be operated even a value other than the initial value (9999) is set in Pr.57 (Restart coasting time). What is the possible cause?
Category : 

Answer

The inverter restart operation is disabled at turn-OFF of the CS signal while a value other than "9999" (with restart) is set in Pr.57. The terminals CS and SD not being shorted may be the cause.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries