FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Operation panel (DU04)
FAQ
Operation panel (DU04)
Is the parameter unit FR-DU04 available in the 700 series inverters?
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
The FR-DU04 can be used in the 700 series inverters, however, some restrictions apply and parameter copy is disabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700