FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Parameter read
FAQ
Parameter read
Pr.77 (Write selection) cannot be read with the parameter unit (FR-PU07). What should I do?For what are they used?
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
By setting Pr.160 (User group read selection ("Extended function display selection" for D700)) to "0", all the parameters can be read.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700