FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter
FAQ
Parameter
How can I read the calibration parameter Pr.C of the inverter parameter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Press the "MODE" key on the operation panel several times to display "P.0" and parameter setting screen.
Then turn the setting dial to display "C..." screen and press the "SET" key.
The display changes to "C---". Turn the setting dial again to the parameter C□ to be calibrated, then press the "SET" key.
Then turn the setting dial to display "C..." screen and press the "SET" key.
The display changes to "C---". Turn the setting dial again to the parameter C□ to be calibrated, then press the "SET" key.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700