FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Offline auto tuning
FAQ
Offline auto tuning
I performed offline auto tuning without running the motor, but I'm not sure if it succeeded. How can I check it?
- Category :
Answer
When auto tuning completes normally, the setting value of Pr.96 (Auto tuning setting/status) is changed to "3". When it is not changed, check the set parameter of auto tuning again.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700