FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA07
FAQ
FR-PA07
When using the enclosure surface operation panel FR-PA07, is the adapter necessary?
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
The adapter is not necessary. Only the dedicated cable FR-CB20□ is required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700