FAQ


FAQAbout Products
 
 - FAQ > Drive Products > Inverters-FREQROL > FR-PA02
FAQ
FR-PA02
      Can I use the operation panel used in the FR-E500 by setting Pr.146 (Built-in potentiometer switching) to "0"?
    
  - Category :
Answer
    The operation panel FR-PA02 requires the optional FR-E5P (control panel rear cover and adapter set) and connection cable FR-CB20□. 
Check that Pr.146 (Built-in potentiometer switching) is set to "0".
Otherwise, the built-in potentiometer of the FR-PA02 cannot be used.
    Check that Pr.146 (Built-in potentiometer switching) is set to "0".
Otherwise, the built-in potentiometer of the FR-PA02 cannot be used.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ