FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200 > Plug-in options
FAQ
Plug-in options
Can I reuse the plug-in option for the FR-A200E?
- Category :
Answer
You cannot reuse the plug-in option for the FREQROL-A200 and A100 series.
You must use one of the following three plug-in options dedicated to the FREQROL-V200:
Note that these dedicated options cannot be used with the FREQROL-A100/A200 series.
- FR-VPA (additional I/O function)Additional input 6 points, additional analog input 1 pint, orientation control, additional output 3 points, long distance cable (50 m to 100 m) power supply, encoder pulse output (open collector)
- FR-VPB (position control function)Position control, additional analog input 1 point, RS485 interface, long distance cable (50 m to 100 m) power supply, encoder pulse output (line driver)
- FR-VPC (digital 12-bit input)Encoder pulse output (line driver, A and B only), long distance cable (50 m to 100 m) power supply, digital 12-bit input, motor thermistor interface, additional analog input 1 point
You must use one of the following three plug-in options dedicated to the FREQROL-V200:
Note that these dedicated options cannot be used with the FREQROL-A100/A200 series.
- FR-VPA (additional I/O function)Additional input 6 points, additional analog input 1 pint, orientation control, additional output 3 points, long distance cable (50 m to 100 m) power supply, encoder pulse output (open collector)
- FR-VPB (position control function)Position control, additional analog input 1 point, RS485 interface, long distance cable (50 m to 100 m) power supply, encoder pulse output (line driver)
- FR-VPC (digital 12-bit input)Encoder pulse output (line driver, A and B only), long distance cable (50 m to 100 m) power supply, digital 12-bit input, motor thermistor interface, additional analog input 1 point
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-V200