FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A100 > New function of EXCELLENT
FAQ
New function of EXCELLENT
What are the new function of the A100E compared with the A100?
- Category :
Answer
The new function includes:
- PI control function
- Cumulative energy monitor (monitor accuracy: approximately ±25% of full scale value)
- Response current limit operation is improved.
- Extended carrier frequency setting range (0.7 to 14.5 kHz)
- PI control function
- Cumulative energy monitor (monitor accuracy: approximately ±25% of full scale value)
- Response current limit operation is improved.
- Extended carrier frequency setting range (0.7 to 14.5 kHz)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100