FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Network operation
FAQ
Network operation
Can I switch between external operation and network operation by setting Pr.182 (Terminal RH function selection) to "66" (External-NET operation switching)?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes.
With the setting "66", you can choose NET operation when X66 is ON, and external operation when X66 is OFF.
With the setting "66", you can choose NET operation when X66 is ON, and external operation when X66 is OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700