FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Parameter setting
FAQ
Parameter setting
I want to set the frequency to 50 Hz using an external frequency setting potentiometer (potentiometer).
Which parameter should I set?
Also, what should I do to prohibit frequencies higher than 50 Hz from being set?
Which parameter should I set?
Also, what should I do to prohibit frequencies higher than 50 Hz from being set?
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
Set Pr.125 (Terminal 2 frequency setting gain frequency) to "50 Hz".
Set Pr.1 (Maximum frequency) to "50 Hz".
Set Pr.1 (Maximum frequency) to "50 Hz".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700