FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > 10 VDC voltage from terminal 10
FAQ
10 VDC voltage from terminal 10
I cannot get 10 VDC voltage from the terminal 10 even after changing Pr.73 (analog input selection) to "0" (for 0 to 10 V input). Is this a failure?
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
Setting Pr.73 to "0" does not generate 10 VDC output.
The inverter itself only has 5 V at the terminal 10.
Setting this parameter to "0" allows 10 V input between the terminals 2 and 5 from an external power supply. The FR-A700/F700 (P) can output 10 VDC voltage from the terminal 10E.
The inverter itself only has 5 V at the terminal 10.
Setting this parameter to "0" allows 10 V input between the terminals 2 and 5 from an external power supply. The FR-A700/F700 (P) can output 10 VDC voltage from the terminal 10E.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700