FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Frequency setting
FAQ
Frequency setting
Can I set the inverter frequency to 120 Hz or higher?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
You can set the running frequency up to 400 Hz.
It depends on the specifications of the motor used whether or not operation with a frequency of 120 Hz or higher is available.
Such operation is available with a high-speed motor.
Use Pr.18 (Maximum frequency) to set the maximum frequency.
It depends on the specifications of the motor used whether or not operation with a frequency of 120 Hz or higher is available.
Such operation is available with a high-speed motor.
Use Pr.18 (Maximum frequency) to set the maximum frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700