FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
When setting the frequency, I set a frequency with the setting dial, press the SET key, and then press the RUN key to operate the inverter. Can I change the frequency during operation?
Currently, I stop the inverter before changing the frequency.
Currently, I stop the inverter before changing the frequency.
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
Even while the inverter is operating, you can use the setting dial to change the frequency and then press the SET key and the inverter operates at the new frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700