FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency, monitor setting
FAQ
Frequency, monitor setting
Using external signals for operation allows for monitoring the running frequency, and I want to continuously monitor the setting frequency.
How should I configure the setting?
How should I configure the setting?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Set Pr.52 (PU/DU main display data selection) to "5".
Set the monitor as the third monitor, frequency -> current -> setting frequency.
Set the monitor as the third monitor, frequency -> current -> setting frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700