FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > RS-485 communication
FAQ
RS-485 communication
I want to perform RS-485 communication. 1. Is it correct to set Pr.117 for "n1" (Station number) of the FR-S500 for the D700/E700/F700PJ series?
2. Is it correct to set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-D700/E700/F700PJ?
3. Are there any other parameters to set?
2. Is it correct to set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-D700/E700/F700PJ?
3. Are there any other parameters to set?
- Category :
Answer
1. You can set Pr.117 for "n1" (Station number) of the FR-S500 for the D700/E700/F700PJ series.
2. You can set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-E700.
3. Change Pr.79 (Operation mode) to "2".
2. You can set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-E700.
3. Change Pr.79 (Operation mode) to "2".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ