FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Output frequency monitor value
FAQ
Output frequency monitor value
After performing auto tuning, the output frequency monitor value was higher than the setting frequency at the operation.
Why is this?
How can I return the inverter to V/F control?
Why is this?
How can I return the inverter to V/F control?
- Category :
Answer
When running the inverter after auto tuning, the frequency setting value is increased by the amount of the motor slippage, resulting in a higher monitor value.
To return to V/F control, return Pr.80 (Motor capacity) and Pr.811(Number of poles) to "9999".
To return to V/F control, return Pr.80 (Motor capacity) and Pr.811(Number of poles) to "9999".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700