FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Terminals P1 and P
FAQ
Terminals P1 and P
When using the brake unit FR-BU2, should I remove the jumper between the terminals P1 and P?
Should I set Pr.30 = "0"?
Should I need to set a percent value in Pr.70?
Should I set Pr.30 = "0"?
Should I need to set a percent value in Pr.70?
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
Removal of the jumper between the terminals P1 and P is not necessary unless you are using the DC reactor.
Set Pr.30 = "0" when using the brake unit.
Since setting Pr.30 = "0" invalidates the setting of Pr.70, you do not have to set it.
Set Pr.30 = "0" when using the brake unit.
Since setting Pr.30 = "0" invalidates the setting of Pr.70, you do not have to set it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700