FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > FR-A500 main circuit wire types
FAQ
FR-A500 main circuit wire types
The "Cable and Solderless Terminal" section under "Installation and Wiring" of the FR-A500 Instruction Manual instructs to "Use copper wires (rated at 75 deg C)".
This note is only found in the FR-A500 Instruction Manual and the catalog of the FR-A500. Similar materials of other types do not have this note but just say "Heat-resistant wires are recommended".
To what extent and why is this type of wire necessary?
This note is only found in the FR-A500 Instruction Manual and the catalog of the FR-A500. Similar materials of other types do not have this note but just say "Heat-resistant wires are recommended".
To what extent and why is this type of wire necessary?
- Category :
Answer
Since the UL standard defines to "Use copper wires (rated at 75?C)", we also recommend the same type of copper wire.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-A500