FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Pulse train output of terminal FM
FAQ
Pulse train output of terminal FM
I utilize the pulse train output from the inverter's terminal FM to display the rotations per minute display with GOT.
The full-scale value should be 1440 pulses/sec, however, the display value differs in no load, full load, and overload. What is the possible cause?
The full-scale value should be 1440 pulses/sec, however, the display value differs in no load, full load, and overload. What is the possible cause?
- Category :
Answer
Under Advanced magnetic flux vector control, the output frequency varies due to slip compensation. This may cause the output frequency monitor value to change and the pulse count varies accordingly.
Also, under V/F control, the output frequency can change due to stall prevention operation and the output pulse count can decrease.
Also, under V/F control, the output frequency can change due to stall prevention operation and the output pulse count can decrease.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500