Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22077
  • Release Date : 2018/08/22 16:30
  • Print

Switching between forward and reverse rotations

How does the inverter operate when the STF signal is turned OFF and then the STR signal is turned ON within the deceleration time?
Is it OK to use the inverter in such a way?
Category : 

Answer

When you switch the inverter to the reverse rotation while it is rotating in the forward direction, it decelerates to stop over the deceleration time (set with Pr.8), and then starts rotating in the reverse direction. After switching to the reverse rotation, the inverter accelerates to the specified speed over the acceleration time (set with Pr.7).
Therefore, it is OK to input the reverse signal while the inverter is rotating in the forward direction.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries