Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22084
  • Release Date : 2018/08/22 16:30
  • Print

Can I drive multiple motors with a single inverter?

Can I drive two 0.4 kW motors and one 0.1 kW motor with a single inverter?
Category : 

Answer

You can drive multiple motors with a single inverter.
However, since the inverter cannot determine the current of each motor, the electronic thermal O/L relay cannot be used.
Therefore, you need to attach an external thermal for each motor for protection.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries