FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Inverter stop-on-contact control
FAQ
Inverter stop-on-contact control
I want to implement stop-on-contact control with the inverter.
I also want to connect the inverter and programmable controller via CC-Link.
Can I realize both of them simultaneously?
I also want to connect the inverter and programmable controller via CC-Link.
Can I realize both of them simultaneously?
- Category :
Answer
Use the FREQROL-A500 series inverter with the optional FR-A5NC.
Then, you can implement both of stop-on-contact control and CC-Link operation.
Then, you can implement both of stop-on-contact control and CC-Link operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500