FAQ


FAQAbout Products
 
 - FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77MS > Speed limit value
FAQ
Speed limit value
      When the speed limit value is changed, does that change affect a command speed lower than the speed limit value?
    
  - Category :
- 
      - FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Simple Motion Modules > RD77MS
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Simple Motion Modules > RD77GF
- FAQ > Controllers > Motion Controllers > MELSEC iQ-F Series > Simple Motion Modules > FX5SSC
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77GF
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75M
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD74MH
 
Answer
    No, there is no impact on the command speed.
However, the actual acceleration/deceleration time are affected by the change.
    However, the actual acceleration/deceleration time are affected by the change.
- Product Name
- Simple Motion module/
 Positioning module
- Series
- MELSEC iQ-R
 MELSEC iQ-F
 MELSEC-Q
 MELSEC-L