Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24780
  • Release Date : 2019/02/27 15:58
  • Print

COM terminal for outputs

There are multiple COM terminals (starting from COM0) for outputs.
How do these terminals differ?
Category : 

Answer

For output terminals of a programmable controller, one common terminal is used for 1, 2, 4, or 8 output points. Each common line is assigned with a different common terminal number (starting from COM0).
The common terminal blocks can drive loads of different circuit voltage systems.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?