FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Power supply cable of the input extension blocks for the connector type programmable controllers
FAQ
Power supply cable of the input extension blocks for the connector type programmable controllers
What is the model and connection method of the power supply cable of the input extension blocks for the connector type programmable controllers?
Answer
For the first input extension block connecting to a main unit, use the FX2NC-100BPCB power supply cable provided with the main unit, and supply power from a 24 V DC power supply. For the second or later input block, use the FX2NC-10BPCB1 power supply cable provided with the input extension block, and connect it to either upper or lower power supply connector of the input extension block previously connected.
- Product Name
- MELSEC-F
- Product Category
- FX1NC, FX3GC, FX2NC, FX3UC
- Series
- Main Unit, I/O Extension
May I have your opinion?
Related FAQ
- Input wiring (FX3 series)
- No communication between a programmable controller and a personal computer (GX Developer) after the communication parameters for the RS-232C communication equipment are set
- Extension blocks and units that can be used in the FX3U series
- How to ground programmable controllers
- Using an expansion board and a special adapter together