FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Using a fixed latched (battery backed) type device as a general type device
FAQ
Using a fixed latched (battery backed) type device as a general type device
How can I use a fixed latched (battery backed) type device as a general type device?
- Category :
Answer
Clear the required area with the ZRST instruction by using the initial pulse when the programmable controller is set to RUN. To clear all the latched type devices, turn on M8032 (latch memory all clear).
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
- Current value of the battery voltage in the FX3U/FX3UC series
- Gratis warranty term of the FX programmable controllers
- Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2
- Setting of the FX3U-ENET-ADP Ethernet communication special adapter