Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Differences between the FX3UC-32MT-LT...
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
No : 24956
Release Date : 2019/04/18 14:28
Print
Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
What are differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2?
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
The built-in CC-Link/LT setting differs.
For the FX3UC-32MT-LT, the built-in CC-Link/LT setting is performed with the DIP switch. For the FX3UC-32MT-LT2, the setting is performed using GX Developer.
Product Name
MELSEC-F Series
Product Category
FX3UC
Series
Main Unit, Network/Communication
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
FX3U-ENET-ADP connectable programmabl...
Ethernet-connectable modules in MELSEC-F
Model of the cable provided with the ...
Number of FX3U-ENET-L Ethernet interf...
Maximum length of input wiring
page top
HOME
FAQ