Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Pulse output type of the FX3U-1PG pul...
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
No : 24972
Release Date : 2019/04/23 07:19
Print
Pulse output type of the FX3U-1PG pulse output block
What is the pulse output type of the FX3U-1PG?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Positioning Control
Answer
It is transistor output.
Transistor output specifications are as follows.
・ Rated load voltage 5 to 24 V DC
・ Maximum load current 20 mA or lower
Product Name
MELSEC-F Series
Product Category
FX3U,FX3UC
Series
Positioning Control
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
Changing the JOG speed in the FX3U-20...
Assignment of direction signals durin...
Compliance of the FX programmable con...
Drive products (servo amplifiers) tha...
Number of FX3U-1PG pulse output block...
page top
HOME
FAQ