Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24995
  • Release Date : 2019/04/23 10:40
  • Print

Operation of the first special function unit/block in the FX3UC series

The first special function unit/block does not operate in the FX3UC series.
Category : 

Answer

Usually, unit number of the first special function unit/block is "K0". However, when the main unit is FX3UC-32MT-LT(-LT2), the unit number "K0" is assigned to the built-in master for CC-Link/LT. Specify "K1" for the unit number of the first special function unit/block.
Product Name
MELSEC-F Series
Product Category
FX3UC
Series
Main Unit
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?