Start main contents

Questions

  • No : 22350
  • Release Date : 2018/08/31 14:33
  • Print

AL

Answer

AL (Alarm switch) is a switch which electrically displays tripping state of a circuit breaker.
The markings of the switch are 8/ALa, 96/ALb and 95/ALc.
*When the circuit breaker itself is ON or OFF, 96/ALb and 95/ALc are conductive states.
*When the circuit breaker itself trips, 8/ALa and 95/ALc are conductive states.
Product Name
Internal Accessories
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?