Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22360
  • Release Date : 2018/08/31 14:33
  • Print

How to select at Inverter circuit

How select the rated current for MCCBs/ELCBs installed at upstream inverter circuit.
Category : 

Answer

Basically you have to consider the effect of harmonic waves, but there are two ways as below.
1. Refer to the recommended rated current by inverter manufacturer.
2. Calculate a load current from power supply capacity described in inverter catalog or other materials, and consider 1.4 times of the value or more as the rated current. It may need 2 times or more ,depending on current waves (Distortion factor, Peak factor, Harmonic component).
Product Name
Molded Case Circuit Breakers
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries