Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22375
  • Release Date : 2018/08/31 14:33
  • Print

Time Delay type at the maximum operating time

What is the operating time range of Time Delay type at the maximum operating time?
Category : 

Answer

The maximum operating time of Time-delay type Earth Leakage Circuit Breaker can be switched to 0.45s, 1.0s and 2.0s. The operating time is:
* when it is 0.45s : between 0.15 and 0.45s
* when it is 1.0s : between 0.6 and 1.0s
* when it is 2.0s : between 1.2 and 2.0s
Product Name
Earth Leakage Circuit Breakers
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?