Start main contents

Questions

  • No : 22397
  • Release Date : 2018/08/31 14:33
  • Print

How to use TBM

Answer

It is an internal accessory to test the earth leakage tripping operation by applying voltage remotely. It is possible to make the same control sequence as the SHT of MCCB, and parallel connection of the TBMs is also possible. (While applying the control input voltage, it remains the state as pushing test button) General TBM includes SLT(vertical lead wire terminal block)
Product Name
Internal Accessories
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?