Start main contents

Questions

  • No : 22401
  • Release Date : 2018/08/31 14:33
  • Print

Minimum operating voltage

What is the minimum usable voltage of MCCBs?
Category : 

Answer

Use with 24V, 0.5A or more for AC and DC in normal use. If the breakers are used
less than 24V, use with 6V, 1A or more. Moreover, regular inspection of is required. ( such as movement of dust, check of abnormal temperature rise ,and ON/OFF operation check by handle) since the influence of the contact surface condition is significant in the low-voltage/ low-current.
Product Name
Molded Case Circuit Breakers
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?