Start main contents

Questions

  • No : 22405
  • Release Date : 2018/08/31 14:33
  • Print

ACB test position

What does the test position of Drawout type mean?
Category : 

Answer

The test position is a position where a main circuit is in the "disconnected" state and
only control circuit is in the "connected" state. Control circuit check and ON/OFF operation check can be done without opening/closing a main circuit.
Product Name
Low Voltage Air Circuit Breakers
Series
AE-SW
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?