Start main contents

Questions

  • No : 22424
  • Release Date : 2018/08/31 14:33
  • Print

How to fix conductors/wires

How to fix conductor/wires to the breaker terminal?
Category : 

Answer

Large electromagnetic force will be generated between conductors/wires due to fault currents. To prevent deformation and breakage of circuit breakers and conductors, place the fixing support for a conductor. The position of fixing support shall be within 200 mm from end of a circuit breaker terminal and shall be strong enough to withstand electromagnetic force.
Product Name
Molded Case Circuit Breakers
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?