Start main contents

Questions

  • No : 22434
  • Release Date : 2018/08/31 14:33
  • Print

ELCB reverse connection

Answer

Almost ELCBs can be connected n reverse. Check the item column of specification table "reverse connection (below 230 V AC)" in the catalog. If it says "Possible", ELCB can be connected in reverse and if it says "-", reverse connection is not possible.
Product Name
Earth Leakage Circuit Breakers
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?