Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22437
  • Release Date : 2018/08/31 14:33
  • Print

ACB How to store drawout handle

Where can the drawout handle be stored ?
Category : 

Answer

Set the handle holder to the right side of the drawout frame with the included screw and nut, and store the drawout handle. However, the circuit breaker with mechanical interlock or door interlock is not possible to install it on the drawout frame, then install and store the drawout handle on the other safety areas except ACB.
Product Name
Low Voltage Air Circuit Breakers
Series
AE-SW
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?