FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU > Virtual servomotor
FAQ
Virtual servomotor
Which signals should I check for the operation status of a virtual servomotor?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
Check the following signals.
• Start accept flag (M2001 to M2032)
• Positioning start complete signal (M4000+20n (n: Axis No.-1))
• Start accept flag (M2001 to M2032)
• Positioning start complete signal (M4000+20n (n: Axis No.-1))
- Product Name
- Motion controller
- Series
- MELSEC iQ-R, MELSEC-Q