FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU > Minor error120
FAQ
Minor error120
What is minor error120?
What should I do when it occurs?
What should I do when it occurs?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
Minor error 120 occurs in the following case:
The zero pass signal (M2406+20n) is OFF when the re-movement to the home position is performed by proximity dog, count, and limit switch combined methods, or when the home position return by data set method is started.
Turn the servo motor at least one revolution to pass the zero point.
Execute the home position return after that.
The zero pass signal (M2406+20n) is OFF when the re-movement to the home position is performed by proximity dog, count, and limit switch combined methods, or when the home position return by data set method is started.
Turn the servo motor at least one revolution to pass the zero point.
Execute the home position return after that.
- Product Name
- Motion controller
- Series
- MELSEC-Q