FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU > Acceleration/deceleration time change
FAQ
Acceleration/deceleration time change
Can I change the acceleration/deceleration time during operation?
- Category :
Answer
Yes, the time can be changed during operation by using the acceleration/deceleration time change function.
Set the acceleration/deceleration time change parameter of the servo data and the command generation axis parameters, and execute the following speed change instruction.
(1) Motion SFC program
Speed change request CHGV, CHGVS
(2) Sequence program
Speed change request D(P).CHGV, D(P).CHGVS
Set the acceleration/deceleration time change parameter of the servo data and the command generation axis parameters, and execute the following speed change instruction.
(1) Motion SFC program
Speed change request CHGV, CHGVS
(2) Sequence program
Speed change request D(P).CHGV, D(P).CHGVS
- Product Name
- Motion controller
- Series
- MELSEC-Q