Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23572
  • Release Date : 2018/09/14 15:09
  • Print

Speed change during operation

How do I change the speed during operation?
Category : 

Answer

Specify the target axes during operation, and execute the following speed change request instruction.
(1) Motion SFC program/Motion program
    Speed change request CHGV
(2) Sequence program
    Speed change request S(P).CHGV
Product Name
Motion controller
Series
MELSEC-Q
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?