Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23574
  • Release Date : 2018/09/14 15:09
  • Print

Speed change during operation

How do I change the speed during operation?
Category : 

Answer

Specify the target axes during operation, and execute the following speed change request instruction.
(1) Motion SFC program
    Speed change request CHGV, CHGVS
(2) Sequence program
    Speed change request D(P).CHGV,D(P).CHGVS
Product Name
Motion controller
Series
MELSEC-Q
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?