Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23578
  • Release Date : 2018/09/14 15:09
  • Print

CUP type of stand-alone Motion controller

What PLC CPU specification is equivalent to that of the stand- alone Motion controller?
Category : 

Answer

The following shows the specification for the PLC CPU area.
Q170MSCPU: Equivalent to PLC CPU "Q03UDCPU"
           • Program capacity: 30k steps
           • LD instruction processing speed: 0.02μs
Q170MSCPU-S1: Equivalent to PLC CPU "Q06UDHCPU"
           • Program capacity: 60k steps
           • LD instruction processing speed 0.0095μs
Q170MCPU: Equivalent to PLC CPU "Q03UDCPU" I53 Program capacity: 20k steps
           • LD instruction processing speed 0.02μs
Product Name
Motion controller
Series
MELSEC-Q
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?