Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22263
  • Release Date : 2018/08/30 13:48
  • Print

Input wiring (FX3 series)

Input terminals of the FX3 series are wired and the "X0" terminal and the "0V" terminal are short-circuited. However, the input does not turn on.
Category : 

Answer

For the sink input, the "S/S" terminal and the "24V" terminal are needed to be short-circuited.
Product Name
FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
FX3S, FX3G, FX3GC, FX3U, FX3UC
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?