Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22277
  • Release Date : 2018/08/30 13:48
  • Update : 2019/02/19 08:47
  • Print

How to set battery-less operation(FX3U/FX3UC)

Answer

To perform battery-less operation in the FX3U/FX3UC series, set parameters using GX Works2(or GX Developer).

Please refer to the following manual for further details;
FX3U SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode

If you wish to set this operation by using a sequence program, please refer to the following manual for further details;
FX3S/FX3G/FX3GC/FX3U/FX3UC SERIES PROGRAMMING MANUAL - Basic & Applied Instructions Edition
37.2.10 Battery [BATT (BAT)] LED and [ALM] LED OFF command [M8030]
Product Name
FX3U, FX3UC
Product Category
Main unit, Accessories, Options, Engineering Software, GX Developper, GX Works2
Series
FX3U, FX3UC
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?