Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22279
  • Release Date : 2018/08/30 13:48
  • Update : 2019/02/14 10:05
  • Print

How to use variable analog potentiometers in FX3S

I would like to know how to use variable analog potentiometers in a FX3S series.
Category : 

Answer

Numerical value data 0 to 255 corresponding to the scale position is stored in the special data register.
You can create the analog timer (volume type) by specifying the stored value as the indirect specification value of the timer.
  • VR1 → D8030 (Integer 0 to 255)
  • VR2 → D8031 (Integer 0 to 255)
Product Name
FX3S
Product Category
Main unit, Analog Control
Series
FX3S
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?